DOUT#.SOURCE

Description

Gets or sets the digital output source.

Value Description
0 - User User controls the output value using DOUT#.STATEU
1 - Action Table Action table controls the output value
2 - FieldbusClosedA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Fieldbus controls the output value

Examples

Usage

When DOUT#.SOURCE = 0 (User), then DOUT#.STATE will be controlled by DOUT#.STATEU.

When DOUT#.SOURCE = 1 (Action table), then DOUT#.STATE will be controlled by the assigned action, if any.

When DOUT#.SOURCE = 2 (Fieldbus), then DOUT#.STATE will be controlled by the fieldbus output control object 3601h sub 1.

Code

Changing output state with STATEU and then changing SOURCE to be action table with no action configured:

--> DOUT1.SOURCE
0 //user
--> DOUT1.STATE
0
--> DOUT1.STATEU 1
--> DOUT1.STATE
1
--> DOUT1.SOURCE 1 //action table
--> DOUT1.STATE
0

Context

For more information see Digital Inputs and Outputs.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Read/Write
Units N/A
Range 0 to 2
Default Value 0
Data Type Integer

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported

Fieldbus Information

Fieldbus Parameter Index Sub-Index Data Type Float Scale Units Access PDO Mappable
EtherCATClosedEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen DOUT1.SOURCE 0x360A 0x1 USINT - - RW False
DOUT2.SOURCE 0x360B 0x1 USINT - - RW False
DOUT3.SOURCE 0x360C 0x1 USINT - - RW False
DOUT4.SOURCE 0x360D 0x1 USINT - - RW False
DOUT5.SOURCE 0x360E 0x1 USINT - - RW False
DOUT6.SOURCE 0x360F 0x1 USINT - - RW False
DOUT7.SOURCE 0x3610 0x1 USINT - - RW False
DOUT8.SOURCE 0x3611 0x1 USINT - - RW False
DOUT9.SOURCE 0x3612 0x1 USINT - - RW False

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen